- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a remote repository for a project
Create a remote repository to enable multi-user collaboration on a project.
- Create a blank remote repository with tools supplied by the supported version control provider.IMPORTANT: The remote repository cannot contain any files, including theREADME,.gitignore, andLICENSEfiles.
- Create an initial project named the same as the repository. See Create a project from a remote repository.IMPORTANT: The project and repository names must match, including capitalization.For GitLab projects, make sure theFactoryTalk Optixproject name, the GitLab project name, and the GitLab project slug match, including the capitalization.
remote repository
Provide Feedback