Third-party .NET libraries
Extend the C# programming language capabilities using third-party .NET libraries.
IMPORTANT:
FactoryTalk Optix Studio
supports only .NET libraries with the .NET Standard 6.0 destination framework.Add a third-party library in the editor of your choice. See Add a third-party library to the Visual Studio project and Add a third-party library to the Visual Studio Code project.
Provide Feedback