Create an Advanced SVG Image
Prerequisites
Download the star_rectangle.svg image.
- To create an Advanced SVG Image
- InProject view, right-clickMainWindow (type)and select .
- Double-clickMainWindow (type).
- Double-click the empty image on the canvas.
- SelectImport file(s)Import file(s), select the file to import and then chooseSelect.
Provide Feedback