Delete a method from an event
Delete an event to remove the event and the event methods from the project. You cannot delete the default events for a pre-configured element.
- InProject view, select an object.
- InPropertiesunderEvents, expand the user-defined event.
- Select the event and then pressDelete.
The event is removed from the project.
delete method
Provide Feedback