Global methods for variables
Use variable commands to modify variable values at runtime.
Increment value
Increases the value of a variable by a set value.
Argument | Description |
---|---|
VariableToModify | Variable for which to increment the value |
Delta | Value of increase of a variable |
ArrayIndex | (Only for array) Cell to modify |
Set bit value
Sets the value of a specific bit of a variable.
Argument | Description |
---|---|
VariableToModify | Value to modify |
Value | Value to set |
ArrayIndex | (Only for array) Cell to modify |
BitIndex | Specific bit to modify |
Set variable value
Specifies the value of a variable.
Argument | Description |
---|---|
VariableToModify | Value to modify |
Value | Value to set |
ArrayIndex | (Only for array) Cell to be modified |
Toggle
Inverts the value of a Boolean variable.
Argument | Description |
---|---|
VariableToModify | Variable for which to invert the value |
ArrayIndex | (Only for array) Cell to modify |
Toggle bit
Inverts the value of a specific bit of a variable.
Argument | Description |
---|---|
VariableToModify | Variable for which to invert the value |
ArrayIndex | (Only for array) Cell to modify |
BitIndex | Specific bit to modify |
increment
set bit
set variable
toggle
toggle bit
Provide Feedback