- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Create a graphic object from a type
Create an instance of an object from a predefined graphic object type or a custom graphic object type.
- InProject view, inUI, double-click the container to contain the object.The container opens in the editor.
- FromType view, select the folders to navigate to the object type and then and drag the object to the editor.TIP: You can also right-click a container inProject viewand select the object to add from theNewcontext menu.
An instance of the object is added to the container. If you add more instances of the same object to the same container, the object name is appended with an increment number.
Provide Feedback