Containers

Containers

Use container objects to structure your application and create user interface navigation.
Object
Description
Container for objects that constitute a specific widget. By default, each new panel has a fixed width and height and is aligned with the top-left corner of the parent object.
Container for objects that constitute a specific interface. By default, each new screen stretches to cover the entire parent object.
Container that automatically arranges objects horizontally next to each other.
Container that automatically arranges objects vertically next to each other.
Container that arranges objects in a grid.
Container that automatically scales its children objects when the container aspect ratio changes.
Container that displays other panels based on the application logic.
Container that contains other panels and automatically organizes panels into tabs that you can navigate.
Button that opens and closes a panel when selected.
Root container. In a Presentation Engine, you can set Window to specify the initial user interface at runtime.
A modal window that does not allow interaction with other interface components until it is closed.
A window that displays in response to an event.
Panel that can scroll to display content larger than the panel size.
Container that includes expandable content blocks.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal