Add a screen type
Create a Screen type in the
Screens
folder.Prerequisites
- InProject view, right-clickScreensand select .
- (optional) InProperties, set the screen type properties.TIP:By default, each new screen stretches to cover the entire parent object.For more information, hover-over the properties.Each instance of the screen type uses these properties as default properties.
- (optional) Add objects to the screen type.Each instance of the screen type includes the children objects of the screen type. You cannot remove objects inherited by screen instances from screen types.
Provide Feedback