Create an Advanced SVG Image object
Add an Advanced SVG Image object representing a conveyor and dynamically link its chassis representation to the alarm.
Prerequisites
Download and extract the SVG 1.2 Tiny image.
- To create an Advanced SVG Image object
- Create the image object:
- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the image, select , and enterConveyorImage.
- Configure the image object:
- Double-click the empty image on the canvas.
- SelectImport file(s)Import file(s), select the file to import and then chooseSelect.
- Under, setIDvalue toConveyorChassis.
- Create a complex dynamic link betweenValueandConveyorChassisMalfunctionAlarmVariablewith the use of a conditional converter.
- True value
- #f51616
- False value
- #000000
- Condition DynamicLink
For more information about dynamic links, see Create dynamic links.
Provide Feedback