Develop filterable data grids
Develop a grid that displays motor parameters and a grid that display motor manufacturing details.
NOTE:
Download a sample project:
FilterableDataGrids.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
TIP:
For examples on how to filter motor parameters with queries, see Numeric data query examples.
Provide Feedback