FactoryTalk Remote Access Manager Best Practices

FactoryTalk® Remote Access
Manager Best Practices

Use the following tips for proper usage of
FactoryTalk® Remote Access
.
• In the case of software installations on Windows devices, configure a firewall in the network (best if a hardware firewall) so that all connections from the Internet to the device are blocked. Only one outgoing port should be used by
FactoryTalk® Remote Access
(TCP port 443, 80 or 5935) and kept open from the device to the Internet.
• Windows devices should only run controlled and safe software.
• Update the
FactoryTalk® Remote Access
software in case security improvements are released.
• Given a given proper, static and controlled industrial environment, an antivirus software can be avoided.
• A strong administrator password change per IEC 62443-3-3 is enforced to register a Router to an organization. Keep the administrator password safe and do not share it with unauthorized personnel.
FactoryTalk® Remote Access
routers can be connected to the Internet through their WAN port.
FactoryTalk® Remote Access
routers do not enable any service through that port and will only need an outgoing connection through to the configured outgoing port (TCP port 443, 80 or 5935). They do not expose any surface to known attacks from the outside. The latest version of the firmware stack against new kinds of attacks is periodically tested. However, for best security, an additional specialized hardware firewall provides the best protection from the outside.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.