Configure FLEX I/O Digital Modules
Use the default configuration supplied with your FLEX I/O modules, or use the
Logix Designer
application to configure a module specific to an application to either:- Accept the default configuration for your module
- Write point-level configuration specific to your application
To configure a FLEX I/O digital module:
- Right-click the desired module to configure, and selectProperties.
- Enter the configuration information.
- Click OK to save the changes and close the dialog box.
It is also acceptable to configure a module when creating a module. If not using the default configuration established for a FLEX I/O module, configure it according to the desired specifications. Select one of the following module types for the module-type configuration.
Input | Output | Combo |
1794-IB16D | 1794-OB16D | |
Provide Feedback