Specify scaling
To specify scaling:
- Select theScalingtab.
- For any changes to take effect, selectOKorApply.In this field:Specify:PV unscaled maximumEnter a maximum PV value (.MAXI) that equals the maximum unscaled value received from the analog input channel for the PV value.PV unscaled minimumEnter a minimum PV value (.MINI) that equals the minimum unscaled value received from the analog input channel for the PV value.PV engineering units maximumEnter the maximum engineering units corresponding to .MAXI (.MAXS).PV engineering units minimumEnter the minimum engineering units corresponding to .MINI (.MINS).CV maximumEnter a maximum CV value corresponding to 100% (.MAXCV).CV minimumEnter a minimum CV value corresponding to 0% (.MINCV).Tieback maximumEnter a maximum tieback value (.MAXTIE) that equals the maximum unscaled value received from the analog input channel for the tieback value.Tieback minimumEnter a minimum tieback value (.MINTIE) that equals the minimum unscaled value received from the analog input channel for the tieback value.PID InitializedIf you change scaling constants during Run mode, turn this off to reinitialize internal descaling values (.INI).
Provide Feedback