Online operations in the properties dialog box Parameters tab
When online with the controller, these guidelines apply for the properties dialog box
Parameters
tab.- Can create parameters and make connections.
- Cannot delete a connection that contains an InOut parameter.
- Cannot delete a parameter that is referenced in any connections.
- Can make edits on the Parameters tab when the controller is online in Remote Run mode. For safety controllers or when the controller is in Hard Run mode, the Parameters tab grids are read only.
Provide Feedback