Use CIP Generic Messaging
ControlLogix
modules have services that can be invoked and data that can be retrieved directly from the module using an MSG instruction and choosing the CIP Generic message type.Select a topic below for more information about some common operations that you may want to perform with CIP Generic messaging. For other operations that are available from each module, see your hardware manual for the module.
Provide Feedback