Configure controller routing
Complete this procedure before importing tags from Beckhoff ® TwinCAT® controllers.
- On the TwinCAT® controller machine:
- Obtain the AMS Net Id value.TIP: You will use the AMS Net Id value later when configuring a communication driver inFactoryTalk Optix Studio.
- Add a route for each device connected to the controller. Use these settings:
- Address Info. Enter the IP address of the target device for aFactoryTalk Optix Application.
- AmsNetId. The same address as in Address Info with.1.1appended at the end.
- Target route. Set to Static.
- Remote route. Set to None/Server.
- SecureADS. Disable.
For more information, refer to the product documentation.
route
beckhoff
Provide Feedback