Runtime entitlements

A runtime entitlement lets you access and run the 
FactoryTalk® Optix
application in a 
Microsoft Windows®
or Linux environment. You can select the runtime entitlement that is aligned to the specific requirements of your application. Runtime entitlements are sold in packages that include a feature token. Different runtime features are assigned a feature token value, so that any set of features can be used in an application. The application features and total feature tokens used defines the runtime license size required. For more information on sizing your application, see Runtime sizing tool.
The
FactoryTalk® Optix Studio
provides a development environment for creating and testing HMI projects before deploying them to the device. The version is important for ensuring compatibility between the project and the runtime environment and may be useful for troubleshooting issues related to project development and deployment.

Typical runtime entitlements

The following table shows typical features that could be used in a
FactoryTalk® Optix
applications.; you can use any combination of features in an application, as long as the runtime license covers the total feature tokens required.
FactoryTalk® Optix
runtime entitlements and typical applications
Feature
Station—Lite
Station—Standard
Station—Pro
X-Small
Small
Medium
Large
X-Large/Unlimited
Controller connectivity, acting OPC UA server, and basic display
Single Rockwell Automation controller
Yes
Yes
Yes
Yes
Yes
OPC server (1 connected client)
Yes
Yes
Yes
Yes
Yes
Data logging with local database
Yes
Yes
Yes
Yes
Yes
HMI graphics
Yes
Yes
Yes
Yes
Yes
Basic HMI that includes all X-small capabilities plus:
Third-party controller support
Yes
Yes
Yes
Yes
Alarming
Yes
Yes
Yes
Yes
Basic reporting
Yes
Yes
Yes
Yes
Security with Active Directory
Yes
Yes
Yes
Yes
HMI station that includes all Small capabilities plus:
Multiple controllers (Rockwell Automation or third party)
Yes
Yes
Yes
Recipes
Yes
Yes
Yes
OPC UA client
Yes
Yes
Yes
Comprehensive HMI station that includes all Medium capabilities plus:
HTML5 HMI up to three web clients
Yes
Yes
Audit signatures
Yes
Yes
Database—ODBC with one database connection
Yes
Yes
Extensible HMI station that includes all Large capabilities plus:
Multiple OPC UA client connections
Yes
OPC UA server for multiple clients
Yes
Database—ODBC with multiple database connections
Yes
Unlimited station runtime entitlements also available
Yes
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.