Embedded Edge Compute module

The Embedded Edge Compute module is a chassis-based module that can communicate directly with Logix controllers, and has read and write access to all controller tags through the backplane and front Ethernet port. The Embedded Edge Compute module enables
FactoryTalk® Optix Studio
, a development platform for creating HMI and Internet of Things (IoT) applications. The Embedded Edge Compute module contains a
FactoryTalk® Optix
XS runtime license with five tokens, and a
FactoryTalk® Remote Access
Runtime Pro license.
For more information about how to use your Embedded Edge Compute module, see the user manual, publication 1756-UM021.
Embedded Edge Compute module
This image shows a ControlLogix Embedded Edge Compute module.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.