Proxy

Proxy connection can be configured through the
Connection Settings
Tool.
NOTE: See FactoryTalk Remote Access Manager Tools and Connection Settings for further information on this Tool.
You can choose among three proxy types:
  • None:
    No proxy configuration.
  • HTTP:
    The HTTP proxy supports Basic authentication (BA) or no access authentication method.
    NOTE: Other access authentication methods (for example, DIGEST or NTLM) are not supported.
  • SOCKS5:
     The SOCKS5 proxy does not require any authentication method.
    NOTE: No access authentication method is supported.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.