Logic > Instruction Usage command
Choose this command to launch the
Instruction Usage
window. Use the Instruction Usage
window to view which PlantPAx and process instructions are used in which tasks. This view provides a way to see the overall process execution load on a project for each task.Tip: | This command is only available for PlantPAx controllers. |
Provide Feedback