Open the code editor
Open the code editor to view and edit the code for
FactoryTalk Design Studio
elements.
IMPORTANT:
Changing the name of any object using the code editor does not change all references to that object.
To open the code editor:
- InFactoryTalk Design Studio, open a routine.
- SelectCode editorto open the code editor.
You can also right-click a program element and open the code editor:
- In theExplorerpane, selectSystemto display elements in a program, or selectLibraryto display elements such as smart objects, AOIs, and data types.
- Right-click an element and selectCode editor.
Provide Feedback