Tasks
Create a task to schedule when programs execute. Schedule a task to run continuously, periodically, or when triggered by a specific event. A program executes a set of instructions in a project. Creating a task varies by task type. Task types include:
- Continuous. A continuous task runs continuously in the background through all assigned programs. CPU times not allocated to other operations scan the assigned programs. After the continuous task scans a program, an output update triggers and the task scans the next program.
- Periodic. Periodic tasks perform a function at a specific rate. Multiple periodic tasks may exist where each task is operates at independent rates.
- Event. Event tasks perform a specific function that is triggered by a specified event.
Create up to 1000 tasks.
Provide Feedback