Allocate a FactoryTalk Optix Studio Pro entitlement to your organization

A newly purchased entitlement can be viewed by the purchaser in FactoryTalk Hub. Then, the entitlement must be allocated to the related organization, to be made available to other users as well.
  1. Access FactoryTalkHub.com to view your new entitlement.
  2. In the FactoryTalk Hub page title bar, select , then select
    View Entitlements
    .
    The new entitlement appears at the top of
    All entitlements
    under
    Available for allocation
    .
  3. Verify that the correct organization name appears on the right side of the FactoryTalk Hub title bar.
  4. Locate the entitlement that you want to assign to your organization and select
    Allocate
    next to the entitlement row.
  5. Ensure that the entitlement, organization and allocated entitlements quantity are correct, then select
    Review Allocation
    .
    TIP: Once allocated to an organization, an entitlement cannot be deallocated.
  6. When prompted, confirm the allocation.
    The entitlement is allocated to the organization.
  7. In the upper left corner of the FactoryTalk Hub web page, select
    Home
    .
  8. Select the
    FactoryTalk Optix
    tile.
  9. Authenticate as required. See Authenticate your FactoryTalk Hub account.
  10. At the top of the FactoryTalk Optix landing page, select
    Entitlements
    .
  11. On the
    Entitlements
    page, select
    Organization entitlements
    .
The allocated entitlement appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.