Launch FactoryTalk Optix Studio Pro

Once an entitlement has been allocated, you can launch FactoryTalk Optix Studio Pro from either your desktop or a web browser, having the Pro features enabled in either way.
NOTE: Without any entitlement allocation, FactoryTalk Optix Studio behaves as FactoryTalk Optix Studio Standard.
NOTE: You can use FactoryTalk Optix Studio Pro if you have been assigned an entitlement or granted a 90-day trial period.
  • Launch FactoryTalk Optix Studio Pro from your desktop
    :
    IMPORTANT: Despite the application icon on the desktop remains unchanged, the Pro features will show up upon valid user login and entitlement allocation.
    1. In the Windows
      Start
      menu, start typing
      FactoryTalk Optix Studio
      or double-click the FactoryTalk Optix Studio icon on your desktop.
    2. Once the application opens, if you are not signed in, select
      Sign in
      from the top bar and sign in with your MyRockwell account credentials.
    3. If you made any changes to your entitlements while working with FactoryTalk Optix Studio, restart the application.
  • Launch FactoryTalk Optix Studio Pro from a web browser
    :
    1. Access FactorytalkHub.com and select the
      FactoryTalk Optix
      tile.
    2. Authenticate as required. See Authenticate your FactoryTalk Hub account.
    3. On the FactoryTalk Optix landing page, select
      Open in Browser
      .
      TIP:
      If you do not have an entitlement for FactoryTalk Optix Studio Pro, a dialog displaying
      Entitlement required
      opens.
      Complete
      Name
      ,
      Email
      , and
      Description
      and then select
      Submit
      .
      You will receive an email to grant you a trial entitlement when your request is approved. Approval can take up to 24 hours. You can download and install the desktop version of FactoryTalk Optix Standard until your FactoryTalk Optix Pro entitlement is approved. When the entitlement is available, repeat the steps above.
    4. Select
      Continue
      to launch FactoryTalk Optix Studio.
      TIP:
      Selecting
      Cancel
      keeps the FactoryTalk Optix landing page open.
      To automatically open FactoryTalk Optix Pro from your last session, select the avatar with your initials in the upper right corner of the landing page, and then in
      Settings
      , select
      Auto open last used workspace
      and select
      Save
      .
      NOTE: Once you launch FactoryTalk Optix Studio Pro from a browser once, it automatically launches the next time you open the FactoryTalk Optix landing page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.