FactoryTalk Optix Studio Standard setup overview
Once you have download
FactoryTalk Optix Studio Standard
from the FactoryTalk Hub and installed it, you can start using it without purchasing an entitlement.- Access FactorytalkHub.com and select theFactoryTalk Optixtile.
- Authenticate as required. See Authenticate your FactoryTalk Hub account.
- On the FactoryTalk Optix landing page, selectDownload.NOTE: See FactoryTalk Optix landing page for further details on this subject.
- Select the checkbox next toFactoryTalk Optix Studioand in the upper right corner, select the first instance ofDownload Nowat the top.
- Scroll to read the EULA and selectAccept and Download.The download progress is displayed in theDownload Manager.
- When the download is complete, in the lower left corner, select the up arrow to selectShow in folderand then double-click the execution file.
- SelectI accept the agreementand complete the setup to install FactoryTalk Optix Studio Standard.
FactoryTalk Optix Studio Standard is installed and ready to use.
Provide Feedback