Current Language Combo Box

Use to switch the currently used documentation language. By changing the selection in the Current Language combo box, the language is dynamically changed for all project documentation. Use of this combo box is the quickest, most convenient way to switch a language dynamically in the project.
Language_with_Content_Icon
This icon indicates that the currently selected language has documentation associated with it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.