Custom Language Configuration dialog box overview

The
Custom Language Configuration
dialog box contains a list of all the custom languages currently supported by the project.
  • Add
    . Click to open the Create Custom Language dialog box in which you specify the name of the custom language you wish to create.
  • Modify
    . Click to open the Modify Custom Language dialog box in which you can change the name and root of an existing custom language. Modify is unavailable until you select a language to modify.
  • Delete
    . Click to open the Delete Custom Language Confirmation Overview dialog box in which you can remove the custom language and any associated documentation from the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.