Error - Failed to undo the check out

An error occurred in the undo of the check out of the file and the undo of the file check out did not occur.
OK
Click this button to return to close the error window.
Help
Click this button for help on this error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.