Failed to schedule the program to the indicated task

Problem scheduling the program to the indicated task.
This may occur if the maximum number of scheduled programs is exceeded.
Cannot schedule more than 1000 programs to a single task. If this limit is exceeded, choose a different task to schedule this program, or remove one of the existing programs from the task.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.