Menu Access to RSNetWorx Software
For ControlNet modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx software is used to:- Save the current network data into the ControlNet project file (*.xc).
- View and edit the network.
- Schedule a ControlNet network.
You must apply any pending edits before you can launch RSNetWorx software for ControlNet.
This option is not enabled until:
- You have specified a ControlNet project file.
- You have specified a slot number and a node number for the ControlNet scanner.
For DeviceNet modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx software is used to:- Save the current network data into the DeviceNet file (*.dnt).
- View and edit the DeviceNet network.
This option is not enabled until:
- You have specified a DeviceNet project file
- You have specified a slot number for the DeviceNet scanner
For EtherNet/IP modules
Right-click the module and select
Launch RSNetWorx
. RSNetWorx software is used to:- View and edit the network.
- Audit an EtherNet/IP network.
You must apply any pending edits on the profile before you can launch RSNetWorx.
This option is not enabled until:
- You have specified a valid EtherNet/IP project file
- You have entered an IP address or host name for the EtherNet/IP scanner
Provide Feedback