Safe Torque Off bypassed
This warning displays when the drive is a CIP Safety drive and Safety State is
Not Configured (Torque Permitted)
or Not Running (Torque Permitted)
.The Safe Torque Off safety function may be bypassed when performing a Motion Direct Command while the safety controller is in Program Mode. The CIP Safety drive allows Motion producing power when Safe Torque Off is bypassed.
Provide Feedback