Assign main and fault routines
Use the
Configuration
tab of the Program Properties
dialog box to assign main and fault routines for your program. To assign main and fault routines:
- From either the Controller Organizer or Logical Organizer, right-click the program to change and chooseProperties.
- Choose the routine to designate as the main routine from theMainmenu in theAssigned Routinesframe.
- Choose the routine to designate as the fault routine from theFaultmenu in theAssigned Routinesframe.
- ClickOK.
Provide Feedback