Change controller properties

Use the settings in
Properties
to change the controller name and description.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , select the controller.
  3. If
    Properties
    is not open, on the pane
    bar, select Properties Icon
    Properties
    .
  4. In
    Properties
    , under
    General
    , change:
    • Name
      . The unique name of the controller.
      TIP: Controller names:
      • Can contain up to 40 valid characters.
      • Can contain only alphanumeric characters and underscores
      • Must begin with a letter or an underscore
      • Cannot contain consecutive underscores
      • Must end with a character other than an underscore
    • Description
      . The description of the purpose of the controller in the system.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.