Create FaultHandler program

Create a program to operate as the controller fault handler. Program tags are automatically created when you create a FaultHandler program.
  1. On the explorer bar, select Execution Icon
    Execution
    .
  2. Right-click the
    Handlers
    folder and select
    New FaultHandler program
    .
  3. In
    New Program
    configure:
    • Name
      . Read-only.
    • Description
      . Enter a description of the program.
    • Create a Main Routine
      . Position the switch Toggle On Position to
      On
      .
    • Main Routine type
      . Select
      Ladder Diagram
      .
  4. Select
    Create
    . The new program and main routine appear in
    System
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.