Count Up (CTU)
The CTU instruction counts upward each time the rung-condition-in transitions from false to true.
When rung-condition-in is set to true and .CU is false, ACC will be incremented by one. When rung-condition-in is false, .CU will be cleared to false.
Available Languages
Ladder Diagram
Operands
IMPORTANT:
Unexpected operation may occur if:
- Output tag operands are overwritten.
- Members of a structure operand are overwritten.
- Except when specified, structure operands are shared by multiple instructions.
Ladder Diagram
Operand | Data Type | Format | Description |
---|---|---|---|
Counter | COUNTER | tag | Counter structure |
Preset | DINT | immediate | Value of Counter.PRE. |
Accum | DINT | immediate | Value of Counter.ACC. |
COUNTER Structure
Mnemonic | Data Type | Description |
---|---|---|
.CU | BOOL | The count up enable contains rung-condition-in when the instruction was last executed. |
.DN | BOOL | The done bit when set indicates the counting operation is complete. |
.OV | BOOL | The overflow bit when set indicates the counter incremented past the upper limit of 2,147,483,647. |
.UN | BOOL | The underflow when set indicates the counter decremented past the lower limit of -2,147,483,648. |
.PRE | DINT | The preset value specifies the value which the accumulated value must reach before the instruction indicates it is done. |
.ACC | DINT | The accumulated value specifies the number of transitions the instruction has counted. |
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Index through arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State | Action Taken |
---|---|
Prescan | The .CU bit is set to true to prevent invalid increments during the first program scan. |
Rung-condition-in is false | Set Rung-condition-out to Rung-condition-in See CTU Flow Chart (False) |
Rung-condition-in is true | Set Rung-condition-out to Rung-condition-in See CTU Flow Chart (True) |
Postscan | N/A |
CTU Flow Chart (False)
CTU Flow Chart (True)
Example
Ladder Diagram
After limit_switch_1 goes from disabled to enabled 10 times, the .DN bit is set to true and light_1 turns on. If limit_switch_1 continues to go from disabled to enabled, counter_1 continues to increment its count and the .DN bit remains set. When limit_switch_2 is enabled, the RES instruction resets counter_1 (clears the status bits and the .ACC value) and light_1 turns off.
Provide Feedback