Develop a motor management dashboard
The UI contains a list of motors and gauges that display speed and acceleration values.
Application example
![](/content/dam/dita/en/factorytalk-optix/current/_images/MotorManagementDashboard.png/_jcr_content/renditions/original)
NOTE:
Download a sample project:
MotorManagementDashboard.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
![](/content/dam/dita/en/factorytalk-optix/current/_images/MotorManagementDashboardDesign.png/_jcr_content/renditions/original)
Select
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback