Enable PowerFlex tags in a project

  1. In Project view, select and in Properties, set up the following PowerFlex parameters:
    • Update rate
    • IPAddress
    • PFType
  2. To create a PowerFlex model, right-click on and execute the GetPowerFlexModel method.
    The model is available in a new directory named with the PowerFlex type, its IP address, and update rate. For example
    PF755TM_10.76.38.210_10sec
    .
  3. To add another PowerFlex drive, repeat steps 1 and 2.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.