Align objects

Align selected objects vertically or horizontally in the Design Area. Aligning objects increases and decreases the margins of the selected items.
  1. In
    Project view
    , double-click a container or select
    Editor
    .
    The editor opens a separate tab.
  2. Select the objects to align.
    TIP: To select multiple objects, hold down
    Ctrl
    and select multiple objects.
  3. In the Design Area toolbar, select the icon to align the selected objects in the Design Area:
    •   Align at the left border.
    •   Aligns at the top border.
    •  Align at the right border.
    •   Align at the bottom border.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.