Base controls

Use base controls objects to implement user interface elements that enable interaction with the application.
Object
Description
Displays text that describes an item.
Inserts and displays text at runtime.
Increases or decreases a numerical value using buttons or keys.
Displays an editable description of an item.
Displays a Boolean value in the form of an on LED or an off LED.
Generates events to perform methods.
Sets and displays a Boolean value.
Sets and displays a Boolean value using select and clear.
Selects a mutually exclusive option in a group.
Sets or displays an integer value within a range of possible values.
Sets or displays an integer value within a range of possible values.
Displays date and time data in a specific input format.
Displays the duration data.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.