XY Chart
Display the value of two-dimensional variables in a graph.
Use case
Graphically represent or set machine processes, for example the cutting profile or the work area within which a machine can operate.
TIP:
You can disable the display of a pen by setting its
Enabled
property to False
.Example
![](/content/dam/dita/en/factorytalk-optix/current/_images/xy_chart.png/_jcr_content/renditions/original)
Provide Feedback