Multistate image

An object that can have multiple image states based on the input value. Each image state may reference a different image and may have a specific opacity. If the input value does not correspond with any image state, the default value is used (first defined state).

Example

State 0: 100% opacity
State 1: 50% opacity
State 3: 25% opacity
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.