Create a variable from a type
Create a variable from a type to have the type automatically assigned to the variable that you create.
- InType view, navigate to the folder that contains the variable type.
- FromType view, drag the variable type intoProject view.An instance of the variable type displays inProject view.
- (optional) InProperties, select, selectDisplay name, and enter the display name.
- (optional) InProperties, select, selectDescription, and enter the description.
Provide Feedback