Reuse objects from the default recipes editor
You can use the objects from the default recipes editor widget as building blocks of a custom recipe management solution.
- InProject view, right-clickRecipesand select .
- Select theRecipesEditorobject and select.LockThe graphical objects associated with theRecipesEditorobject display.
- Develop a custom management recipes interface.For more information, see Recipes editor customization.
- Remove the defaultRecipesEditorwidget that you created in 1.
reuse
Provide Feedback