Delete a role

Delete a role to remove the role and no longer have the assigned users be members of the role.
Delete a role from either the dashboard page or
Project view
.
  1. In the main toolbar, select
    Open dashboard page
    and then select
    Manage users and groups
    .
  2. On the dashboard page under
    Roles
    , select the role or roles to delete
    .
  3. Select
    Delete
    .
    TIP: You can also right-click the role to delete on either the dashboard page or in
    Project view
    and then select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.