Download Runtime Tools on the Runtime device
Runtime Tools are required on any device running a FactoryTalk Optix application.
They include the
License Manager
and FactoryTalk Optix Application Update Service
.Runtime Tools are embedded in OptixPanel
™
Graphic Terminals by standard, so you do not need to download and install them.If you are using a Runtime device, download Runtime Tools from the FactoryTalk Optix landing page. You can download and install Runtime, including License Manager.
- Access the FactoryTalk Optix landing page. See FactoryTalk Optix landing page.
- Authenticate as required.
- On the FactoryTalk Optix landing page, selectRuntime Tools.
- Scroll down toRuntime Tools Releaseto view the Runtime Tools released versions.
- (optional) To view the FactoryTalk Optix release notes, selectRelease Notes.
- (optional) To view the latest changes in FactoryTalk Optix, selectChangelog.
- (optional) To search for a specific Runtime Tools release, type the release number inSearch.
- To download a specific Runtime Tools release, selectDownloadafter the desired version number, .
- Select the checkbox next to theFactoryTalk Optix Runtime Toolsinstallation package and click on the first instance of the symbol in the upper right corner. Eventually, click onDownload Now.
- Scroll to read the EULA and selectAccept and Download.
- Install theRockwell Automation Download Managerlocated in your Downloads folder. To do so, select .Rockwell Automation Download Managerinstalls, runs, and download the Runtime Tools into the specified folder. Download progress is displayed in theRockwell Automation Download Manager.
- To determine the Runtime Tools downloading path, after the path, selectChangeto select a different folder.
- Runtime Tools are ready for installation.
Provide Feedback