Custom service - application example
The
Custom
service allows you to enter a command line that includes a directory path on the user's device to a specific application, and directly runs it through a dialog box.- In, select the sub-device.
- On the right pane, expand the theServicessection to view all of the sub-device services.
- In theServicespane, create or edit an existingCustomservice by clicking respectively thecircled plusorpencilicon.
- If not previously done, set.
- In theCustom Actionfield, enter a directory path along with the file name and extension of the application that you want to run. See the examples below:UltraVNC"<executable>" -connect <IP:Port>"C:\Program Files (x86)\uvnc bvba\UltraVNC\vncviewer.exe" -connect 192.168.0.2:5900TightVNC"<executable>" <IP:Port>"C:\Program Files\TightVNC\tvncviewer.exe" -connect 192.168.0.2:5901SSH via Putty"<executable>" -ssh <user>@<address>"putty.exe" -ssh root@192.168.10.2
- ClickLaunch.TheInteractive AccessTool automatically establishes a VPN connection with the device to which the sub-device is connected. In this way, you are granted access to the device subnet, so you can reach the sub-device and make its service run.
Provide Feedback