Error - Failed to associate the current project with any project under source control
Source control operations will not be available for this project.
OK
Click this button to close the dialog box and open either a copy of the file or a standard, writable project with only the Add to Source Control menu item available.
Help
Click this button for help on this error.
Provide Feedback