Function Block Online Edit Animation
Function block diagram online edit animation values are based on the logic that is currently running in the controller. For example, if the routine from the Test Edits view is currently running, the animation values will reflect the logic in that routine. If you navigate to the Original view while the Test view routine is running, any logic that also exists in the Test Edits view will animate even though the Original view logic is not currently running. This is true because the blocks that exist in both views share the same block tag.
New logic that you add in the Pending Edits view and accept to the controller will only animate when the Test Edit logic executes. Similarly, deleted logic will only animate when the original logic is executed.
Provide Feedback