Message Configuration Dialog Box - Configuration Tab Overview
After you enter the MSG instruction and specify the MESSAGE structure, use the
Message Configuration
dialog box to specify the details of the message.The details you configure depend on the message type you select.
Message Configuration Tab
If the target device is: | Select one of these message types: |
---|---|
Logix 5000 controller | CIP Data Table Read |
CIP Data Table Write | |
I/O module that you configure by using Logix Designer application | Module Reconfigure |
CIP Generic | |
PLC-5 controller | PLC-5 Typed Read |
PLC-5 Typed Write | |
PLC-5 Word Range Read | |
PLC-5 Word Range Write | |
SLC controller MicroLogix™ controller | SLC Typed Rated |
SLC Type Write | |
Block transfer module | Block Transfer Read |
Block Transfer Write | |
PLC-3 processor | PLC-3 typed read |
PLC-3 typed write | |
PLC-3 wood range read | |
PLC-3 wood range write | |
SERCOS module | SERCOS IDN Read/Write |
Provide Feedback