Paste Special > With Configuration

Choose this command to configure and rename a program, Add-On Instruction, User-Defined Data Type, or String before pasting it in the Controller Organizer or the Logical Organizer. You can also use Paste Special with Configuration when pasting a folder in the Logical Organizer. Choosing this command opens the Paste Configuration dialog box.
Paste Special > With Configuration is also available when copying from the Controller Organizer to the Logical Organizer, or vice versa.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.